This is the login for Trane® Connect™ and other Trane® commercial applications. Trane® Connect™ is our secure, cloud-based customer portal to access your building systems to remotely monitor and manage building systems, and conduct routine maintenance.
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
Commercial Real Estate Data Centers Food & Beverage Federal Government Fulfillment Centers Grocery & Supermarkets Healthcare Higher Education High Tech
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
  1. Trane Commercial HVAC
  2. About Us
  3. Newsroom
  4. Applying VRF Systems in Cold Climate Applications

Applying VRF Systems in Cold Climate Applications

Variable Refrigerant Flow (VRF) for Wintry Weather: Six Cold Climate Approaches

This white paper discusses six options contractors and engineers can use to solve derating challenges, even in climate zones 5 and 6:

1. VRF flash-injection technology—injecting a small amount of mixed-phase refrigerant to cool the compressor, allowing it to perform at higher speeds without failing due to friction and heat built-up. This technology creates the opportunity to size units based upon heating loads and use the VRF system as a sole source for heating. For example, CITY MULTI® VRF systems with Hyper-Heating INVERTER® (H2i®) technology can provide up to 100% of heating capacity down to -4°F.

2. Auxiliary heat—using a non-VRF backup system such as electric resistance, baseboard hydronic wall fin radiant heat or duct coils mounted downstream of an air handler. Systems may be set up using a Zone-by-Zone method, in which critical zones are covered by auxiliary heat, while non-critical zones are not. Or using a Global Method, in which all the building’s zones switch the VRF system to auxiliary heat at an adjustable ambient temperature.


3. Sole-source sizing based on heating—oversizing standard VRF systems for extra heating capacity. When using this approach, the designer will likely need to oversize the indoor units as well as the outdoor unit. Otherwise, the indoor units will be unable to use the extra capacity. Be mindful of heating derates as found in the VRF manufacturer’s selection software or engineering manuals when using this method.

4. Oversize DOAS system—a dedicated outdoor air system (DOAS) is typically designed to supply room-neutral air (between 70°F and 75°F) but could be upsized to provide additional heat. With the use of a recirculation air damper, an oversized DOAS can be used for emergency heat or morning warmup during winter.


5. Install outdoor unit inside—limiting derating and weather impacts during severe cold by installing air-source condensers inside the building. In this scenario, air-source condensers are installed in a mechanical room that serves as a recirculation air plenum or a pass-through air plenum, depending on the outdoor temperature. This approach can be expensive due to the number of dampers and louvers required but it allows the facility to locate auxiliary heat in a central location.  

6. Water-source VRF systems—available as heat pumps or with heat recovery, water-source VRF systems are designed for indoor use and deliver greater efficiency and have less derating. It takes less energy to extract heat or reject heat into or out of water, compared to air. Also, a water loop offers a more refined and controlled temperature range, generally between 60°F and 90°F.


Applying VRF Systems in Cold Climates

Download the full whitepaper

All-electric variable refrigerant flow (VRF) systems are positioned to replace fossil fuel burning equipment in almost any climate. Modern VRF systems far exceed the capabilities of conventional heat pumps at cold outdoor temperatures, as low as -31°F. When applied according to best practices and considerations for winter weather, today’s VRF systems can serve as the primary heating and cooling system, without requiring auxiliary heat.

Download the Full Paper

Looking for more?

tc-VRF-electrification-blogthumbnail1.jpg

Blog

Electrifying Buildings with VRF Technology

Heating systems that run on natural gas and other fossil fuels have been keeping America’s buildings warm for decades. But that era may be ending.

Steve Hamlin November 04, 2022

VRF and Ductless Solutions, Decarbonization, Electrification, Blog
Texarkana University HVAC Upgrade Building Front

Customer Story

Texas A&M - Texarkana University HVAC Upgrade

A&M - Texarkana improved student housing with a VRF system and a BAS system that provide consistent temperatures, reduces energy costs, and elevates long term efficiency.

April 28, 2025

Higher Education, VRF and Ductless Solutions, Building Automation, Efficiency, IEQ, Financial Solutions, Customer Story
GCH Mechanical's VRF Innovation

Customer Story

Transforming Comfort: GHC Mechanical’s VRF Innovation for High-End Condominiums

September 23, 2024

VRF and Ductless Solutions, Innovation, Products and Solutions, Contractor, Customer Story
tc-vrf-lab-new-mexico-blog-thumbnail.jpg

Blog

New Mexico's VRF Lab: Sustainability and Training for a Decarbonized Future

May 16, 2024

VRF and Ductless Solutions, Innovation, Blog
View More