This is the login for Trane® Connect™ and other Trane® commercial applications. Trane® Connect™ is our secure, cloud-based customer portal to access your building systems to remotely monitor and manage building systems, and conduct routine maintenance.
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
Commercial Real Estate Data Centers Food & Beverage Federal Government Fulfillment Centers Grocery & Supermarkets Healthcare Higher Education High Tech
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
Trane Helps Bring K-12 Students Back to School with Indoor Air Quality Solutions

October 07, 2020

Offerings address critical school needs for indoor air quality assessments, air and surface cleaning technology and funding support 

SWORDS, Ireland, Oct. 06, 2020 – As the school year progresses in various formats, Trane® – by Trane Technologies (NYSE: TT), a global climate innovator – introduces expanded services to help schools evaluate, implement and fund indoor air quality improvements in their buildings.

Heating, ventilation and air conditioning systems (HVAC) play a critical role in creating proper indoor air quality. ASHRAE® guidelines to address COVID-19 in the reopening of schools indicate that making changes to the operation of HVAC systems can mitigate exposure to airborne contaminants.

“As schools bring back students for part-time or full-time in-person learning, healthy indoor air quality is a chief concern alongside other safety practices including wearing masks and social distancing,” said Donny Simmons, president, Commercial HVAC Americas at Trane Technologies. “HVAC systems, properly applied, are an important aspect of addressing environmental concerns within a school.”

Trane ® Indoor Air Quality Assessment and Isolation Space Evaluation

A thorough assessment is a helpful starting point for schools to understand their indoor air quality needs. The Trane® Indoor Air Quality (IAQ) assessment focuses on four critical pillars of indoor air quality – dilute, exhaust, contain and clean. The fact-based assessment equips school building managers with a clear and cost-effective roadmap for improvements that will bring facilities into alignment with CDC and industry recommendations.

The Trane IAQ Assessment now includes a supplemental isolation space evaluation to help schools better prepare for scenarios where students or staff experience symptoms while on campus. The evaluation can help schools create an isolation space in line with industry recommendations, including stringent guidelines for air exchanges, negative pressurization and other criteria.

Comprehensive Indoor Air Quality Solutions

Trane’s comprehensive suite of solutions address conditions and recommendations across all four critical pillars of indoor air quality, including cleaning the environment to actively reduce the number of microbiologicals that may be in the air or on surfaces. Air cleaning technologies range from high-rated MERV or HEPA filters, to Ultraviolet Germicidal Irradiation (UVGI) and photocatalytic oxidation.

To meet the evolving needs of schools and increased demand for air cleaning solutions, Trane now offers Synexis®-made Dry Hydrogen PeroxideTM (DHPTM) solutions to K-12 schools in the U.S. to help reduce the presence of viruses, bacteria, and mold in the air and on surfaces. Synexis® is the sole developer of the process by which naturally occurring humidity and oxygen are taken from the air to create DHPTM, which reduces the presence of unwanted microbes that may be present in the air and on surfaces, continuously improving indoor air quality and surface cleanliness. Synexis® solutions can be integrated into a school’s existing HVAC system or used as a portable, standalone unit in any room to treat the air and any surface the air touches, making it an ideal application for school isolation spaces, classrooms and high traffic areas like cafeterias and hallways.

“Our customers count on Trane to bring them the best air quality solutions and strategies available, and we’re pleased to expand our portfolio with Synexis® solutions for schools,” said Simmons. “Implementing HVAC best practices and innovative air cleaning technologies, such as Synexis®, are ways schools can go on the offensive to help improve indoor air quality and create more peace of mind for students, faculty, administrators and parents.”

Trane Integrated Funding Solutions

“For many schools, the central issue is not whether they need indoor air quality improvements, but how they will they fund them – especially in a year marked by many other unplanned expenses,” said Simmons. “Trane’s expanded and flexible financing options help school districts move forward with the indoor air quality improvements they need now.”

Trane Integrated Funding Solutions (IFS) includes Leasing and Managed Services Agreement options with deferred payment plans and extended terms for qualifying school districts. Additionally, Trane K-12 experts help schools evaluate the most affordable ways to pay for IAQ upgrades, including leveraging CARES Act funding, grants, utility rebates, and other available resources.

The program is designed to help address schools’ financial constraints by eliminating immediate out-of-pocket expenses, preserving working capital and other forms of credit and delivering fast implementation of needed improvements. With flexible funding support, school districts can make needed upgrades to maintain proper indoor air quality now and help minimize impacts on operating budgets.  

“It’s a complex time for schools, and there is no single solution for all environments,” said Simmons. “Every school may have different needs – and variables – when it comes to indoor air quality. The bottom line is schools should work with a trusted partner and take a strategic, fact-based approach to make the best use of their budget and investments.”

Visit www.trane.com/k12 to learn more about Trane solutions for schools.

Additional Information

There is strong evidence from The American Society of Heating, Refrigerating, and Air-Conditioning Engineers (ASHRAE) and other sources that HVAC technologies can mitigate the risk of exposure to infectious aerosols in built environments; however, the transmission and mitigation of COVID-19 in buildings is yet to be fully tested and confirmed.

# # #

About Trane

Trane – by Trane Technologies (NYSE: TT), a global climate innovator – creates comfortable, energy efficient indoor environments for commercial and residential applications. For more information, please visit www.trane.com or www.tranetechnologies.com.

About Trane Technologies

Trane Technologies is a global climate innovator. Through our strategic brands Trane® and Thermo King®, and our portfolio of environmentally responsible products and services, we bring efficient and sustainable climate solutions to buildings, homes and transportation. Visit tranetechnologies.com.

About Synexis

Founded in 2008, Synexis® LLC is a leader in technologies that achieve microbial reduction in treated spaces and is the sole developer and designer of patented technology that creates hydrogen peroxide gas or Dry Hydrogen Peroxide (DHP™) for occupied spaces. Synexis technology takes what is naturally in the environment, ambient oxygen and humidity, to create Hydrogen Peroxide Gas (H2O2) or DHP.

Synexis DHP technology is patented, and effective at reducing certain bacteria, viruses and mold in the air and on surfaces within occupied spaces where the device has been installed.

The Synexis system is UL Certified [i] to produce no ozone and works continuously without disruptions in normal operations or workflow. Synexis Systems are regulated by the U.S. Environmental Protection Agency and state governments as antimicrobial devices. Accordingly, our Systems are produced in an EPA-registered facility and packaged and labeled in accordance with EPA regulations appearing at 40 CFR 152.500. Synexis® currently holds

13 U.S. patents with 16 pending. [ii],


 

[i] UL Certification numbers: Blade UL E482400 and Sentry UL E495096

[ii] Synexis https://synexis.com/patents/ . US Patent numbers include 8,168,122 | 8,685,329 | 9,034,255 | D744,627 | 9,370,592 | 9,808,013 | D814006 | 9,924,722 | 10,188,766 | 10,232,076 | 10,285,382 | 10,299,482 | D890898

Looking For Parts?

Visit Trane Supply

For General and Corporate Questions:

Contact Us