This is the login for Trane® Connect™ and other Trane® commercial applications. Trane® Connect™ is our secure, cloud-based customer portal to access your building systems to remotely monitor and manage building systems, and conduct routine maintenance.
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
Commercial Real Estate Data Centers Food & Beverage Federal Government Fulfillment Centers Grocery & Supermarkets Healthcare Higher Education High Tech
Hospitality Indoor Agriculture Industrial K-12 Life Sciences Local Government Restaurants Retail Buildings National Accounts
About Us Contact Us Locate a Sales Office
Trane Newsroom Customer Stories Trane Blog Events & Webinars Press Releases

CONTACT A TRANE EXPERT

Find Your Trane Rep
Cyxtera_hq.jpg

Customer Story

Cyxtera Data Center: Energy-Efficient Cooling and Cost Savings

Upgrades to Cyxtera’s chiller plant and pumping system controls led to a decrease in energy consumption of 0.7 kW/ton, resulting in over $2,100,000 in annual energy cost savings.

Location: Weehawken, New Jersey

Industry: Data Centers

Products Used: Chillers, Air Handling, Controls

Services Used: Energy Efficiency Contracting, Energy Management & Controls

Topic: Cost-Saving, Decarbonization, Energy Services

Challenge

Cyxtera Communications leased the Weehawken, New Jersey, data center site (NJ2) in 2001 in part due to its proximity to Wall Street and the New York-New Jersey financial markets. The close location meant Cyxtera could take advantage of near-zero lag time in providing its proximity hosting solution to its customers. The NJ2 facility is a split tower with ten, 300-ton Trane Model RTAA air-cooled chillers—five chillers on each tower, each with a Systecon Inc. pumping system and control panel. However, the original control system did not allow for the kind of comprehensive monitoring and control that a mission-critical data center facility requires.

Jason Garbus, Cyxtera Project Engineer, said, “It’s a critical application and these servers are tied in directly with Wall Street. Ninety percent of the work being handled in this data center is banking. If we lost data center precision cooling for only three to five minutes, temperatures could very quickly go from 70 to 95 degrees, and it would take at least a couple of hours to recover. That could cause all kinds of problems for our clients and their customers. Loss of control and cooling simply cannot be tolerated.”

Solution

Systecon Inc. and Trane commercial systems teamed up to install new Systecon VariPrim™ control panels along with Tracer Summit™ building control units (BCU) to communicate with the facility’s overall Automated Logic building automation system.

Scott Corbin of Systecon said, “The new panels include Allen Bradley SLC-5/5 processors and CTC Parker touch screen interfaces. This new control platform provides much better control—the touch screen is much more user friendly and includes extensive graphics so that operators can easily see system operating conditions. The VariPrime system is also consistent with other Cyxtera facilities. We also installed kW meters on the pumps and data center chillers so that operators can instantly see energy consumption.”

Results

The work began in early March 2009, with a kickoff meeting for everyone involved in the project. A June 15 deadline was set but the job was completed three days early. Garbus remarked, “We had absolutely zero impact on our customers’ transactions and the operation of the data center. We never lost chilled water flow or temperature control, and we completed all of this during normal work hours.

Thanks to the Systecon VariPrime and Tracer Summit BCU upgrades, Cyxtera has better, more precise control of the data center chiller system and is reaping huge energy savings. For example, instead of running all 10 data center chillers at full load all the time, only three chillers on each tower are typically running at any given time—delivering significant energy savings and an 18-month payback for the project. When we analyzed this system, the data center chillers were running at 100 percent capacity and although the design called for 45-degree chilled water, it was delivering 34 to 35-degree chilled water.

In addition to improving the control system, this was a huge energy saving opportunity! We can now match data center chiller capacity to the exact cooling load and reset chilled water temperature back to the original design specifications. As a result, energy consumption dropped from about 2.0 kW per ton of cooling to 1.3 kW per ton, saving about $177,000 per month in energy costs. The project also qualified for $35,000 in rebates from the local utility company. Plus, the data center now has immediate backup capacity if any of the 10 chillers fail.”


  • “With the new Systecon panels and Trane BCUs, the Cyxtera facilities managers now get complete information on the data center chillers and pumps. Before, they simply had on/off information. Now, they get all operating conditions including chilled water temperatures, flow rates, etc.”

    Tony Blunt Trane Project Manager
  • “This project would not have been possible without Cyxtera, Trane, Systecon and the other contractors and suppliers. This team has worked together on several data center projects in the past, so this job went very smoothly. This project was like a family reunion!”

    Jason Garbus Cyxtera Project Engineer
  • “This was literally a perfect and completely seamless project. Using the 200-step procedure, everything went perfectly. It wasn’t just like open heart surgery; it was like heart replacement surgery. We were so impressed that we signed a contract with Trane to further maintain our chiller plant.”

    Mike Sims Director of East Coast Operations for Cyxtera Communications
  • “This project is a perfect example of the synergies that are present when industry leaders like Cyxtera, Trane, Systecon and our contractors/suppliers collaborate towards a common goal. We are very pleased with the outcome.”

    Michelle Hassemer Vice President of Global Operations at Cyxtera Communications
  • “This was the nicest job I’ve ever been involved in. We were very impressed with the Trane and Systecon relationship and how they worked together to ensure the success of the upgrade. Trane and Systecon demonstrate a very high level of competence that gives us great confidence. We know that when they’re on a project with us, those areas of the job don’t need so much oversight. We’re excited to continue working with Trane and Systecon to expand and upgrade another Cyxtera facility that’s right next door to the NJ2 data center.”

    Joe Dones Project Executive for Nova Corporation
  • “Our customers expect 100 percent uptime from our data centers. Our ability to meet this expectation hinges on the capability to provide consistent, effective and reliable data center precision cooling. Cyxtera carries responsibility as stewards of the environment as well as a commitment to provide services in a cost-competitive manner. Energy savings derived from projects such as this both enhance our ability to protect the environment and contribute directly to our success as an enterprise.”

    Michelle Hassemer Vice President of Global Operations at Cyxtera Communications
  • Ozark School District embarked to fix HVAC issues and reduce costs with solar installation
    Solar Installation at Ozark School District Reduces Energy Consumption

    Ozark School District embarked to fix HVAC issues and reduce costs. Solar installation at West Elementary reduced energy consumption by two-thirds, promoting sustainability. 

  • Ozark Public Schools
    LED Upgrades are Expected to Reduce the Missouri School District’s Lighting Costs by 32 Percent

    Ozark Public Schools partnered with Trane for a $14.88M LED lighting upgrade, saving up to 32% on utility costs, enhancing learning, and reducing maintenance.

  • Industrial area of the city, harmful emissions into the atmosphere.
    Navigating Rising Energy Costs from PJM Interconnection’s Capacity Auction

    Learn about the PJM Capacity Auction including key information, timelines, and strategies to mitigate rising energy costs.