Watt's in the News? - Volume 3
A lot of energy-related curricular materials focus on the various types of resources that can be used for electrical generation, but before that electricity can reach the end consumer it has to go through the grid. Just as the terms "producer" and "consumer" are used in life science classes to discuss the flow of matter & energy, these terms are also appropriate for helping students understand the electricity (and other forms of energy) must be moved from a generation site to the end consumer, so infrastructure is needed. (i.e. - electrical grid, natural gas pipelines, etc.)
Meet Dan Whisler, Trane Educator in Residence