Meet Dan Whisler, Trane Educator in Residence
Trane ComfortSite is an extranet site designed to save you time. With your secure login, you can:
This is the login for Trane® Connect™ and other Trane® commercial applications. Trane® Connect™ is our secure, cloud-based customer portal to access your building systems to remotely monitor and manage building systems, and conduct routine maintenance.
Selecting a language changes the language and content on the Trane site.
Latin America
Europe
Asia Pacific
When it comes to energy and technology what we find in textbooks is often old news, so in an effort to help you stay on the cutting edge we will use this BTU Crew™ feature to help provide some of the latest energy-related news and resources you can share with your students. Energy-related topics are in the news every day at local, regional, and/or national levels and using these current events and resources can helps students see the relevance to what they are learning.
Over my years of teaching Environmental Science classes I used the two sets of ecology and economics principles below as the "ten fundamentals" of my class, with discussions of current events and environmental issues all related back to one or more of these principles. It really didn't matter the specific topic as research and discussions related to environmental issues and economics all could be used to help students remember the basics and make connections.
This helped to create a "big picture" perspective for energy-related discussions. In the information age today it takes students just seconds to look up details, but what can they do with this information after they have it? Can they make the connections and think critically or is it a detail they have simply memorized for a test? With an understanding of these ten fundamentals, students will have a good foundation for more detailed discussion of various topics.
When you consider energy-related issues involve environmental concerns and science and economics and politics, etc, then provide opportunities for these findings to be communicated to others in both written and verbal forms...it is easy to see how energy can be used as a great topic for PBL!
One of the best "science" workshops I had the pleasure of attending was actually an economics workshop conducted by the Foundation for Teaching Economics. I was fortunate to attend this training not just once, but twice, and it really helped me develop more of a big picture/critical thinking focus in my classroom. Environmental issues are economics issues and you really can't discuss one without involving the other. The ten fundamentals I used to help build a foundation for Environmental Science are from these two resources:
The Closing Circle
In his 1971 bestselling book The Closing Circle, Barry Commoner suggested that the American economy should be restructured to conform to the unbending laws of ecology. One of Commoner's lasting legacies is his four laws of ecology, as written in The Closing Circle in 1971.
BTU Crew Newsletter Volume #33: Year End Wrap Up
BTU Crew Newsletter Volume #31: Where Does Our Electricity Come From?
Blog
Watt's in the News
K-12
BTU Crew Newsletter Volume #33: Year End Wrap Up
BTU Crew Newsletter Volume #31: Where Does Our Electricity Come From?
BTU Crew Newsletter Volume #28: Reviewing the Big Picture