Making changes to reduce emissions in any of these three scopes is how you achieve decarbonization. Working with an expert, you can determine the appropriate mix of initiatives within this framework to achieve your sustainability goals.
Step 3: Make a Restaurant Decarbonization Plan
Decarbonization for restaurants comes down to three main components: Energy Efficiency, Electrification, and Renewable Energy. Let’s look at what goes into each component.
Energy Efficiency
The goal of energy efficiency is to improve the building’s infrastructure to eliminate waste in your operations. This can be done by upgrading to more efficient equipment, making improvements to limit the heat entering or escaping from the building, or reducing the load it takes to heat or cool the space.
The process of becoming more energy efficient starts with simple, cost-effective measures range from identifying and addressing unnecessarily air leaks to installing sophisticated building automation systems that monitor energy use and waste in real-time. A great way to gain greater restaurant efficiency is to start with an energy assessment.
Upgrading to highly energy efficient equipment, including HVAC and lighting, helps to reduce the overall cost of ownership and may help to improve the energy efficiency within your restaurant. Installing automation equipment allows you to centrally monitor and manage buildings across the country, leading to significant savings. Your HVAC expert can work with you to find ways to pay for building upgrades now by using future energy savings.
Electrification
To create a greener energy grid, electricity is increasingly moving to more renewable energy sources like solar and wind. This means electricity is becoming less emission-intensive across the U.S. One of the best ways to take advantage of these greener energy sources is to electrify your heating and cooling operations. An emerging strategy in decarbonization, you can replace your natural gas boiler system with high-efficiency heat pumps. This single piece of equipment that is used for both heating and cooling will remove nearly all onsite direct emissions from your operations. This is a huge advantage for any restaurant looking to achieve decarbonization goals.
Since energy companies are making significant investments to update the grid, many are incentivizing customers to take advantage. The right expert can help you determine how you can receive reimbursements from energy companies that can go towards paying for electrification updates.
Renewable Energy
Restaurant operators can leverage renewable energy as a tool to reduce emissions while gaining more control over their energy supply. While renewable energy has historically been seen as a “cost premium” to traditional energy sources, there are emerging models that allow buildings to secure renewable energy at a discount to traditional power sources.
There are two main ways to secure renewable energy:
- Onsite: A renewable energy asset or system is installed at the facility and provides energy supply directly to the building.
- Offsite: A commitment is made to an offsite renewable energy asset (likely a large utility-scale development) that allows the owner to recognize the renewable energy attributes.
Restaurant operators should explore all the renewable energy options available to them and identify which one has the best alignment and significant returns to the business.
Restaurant owners and facility managers will have growing pressure to decarbonize their operations in the years to come. There are unique challenges, as well as immense benefits, that come with reducing emissions while not impacting core business operations and customer experiences. Balancing these challenges by developing a roadmap to decarbonization that focuses on creating financially attractive solutions to achieve your goals is a core competency of Trane.
Looking to begin, accelerate or complete your restaurant decarbonization journey? Connect with a Trane restaurant expert to develop a financially attractive solution to meet your sustainability ambition.
About the author
Trevor Joelson, Decarbonization Program Lead – Key Accounts
Trevor Joelson is a program lead for Trane’s decarbonization program for key account customers. Through this program, Trevor collaborates with larger enterprises to define their environmental sustainability objectives and establish initiatives and programs to reduce operational emissions through financially attractive and measurable projects.
Trevor joined Trane through an acquisition of Fellon-McCord in 2016 and has held various roles in corporate energy & sustainability management over the last decade. His subject matter expertise is in the energy markets and how the supply-side of energy connects to the built environment.
Trevor lives with his family in Dallas, TX and is a graduate of the University of Louisville.