This is the login for Trane® Connect™ and other Trane® commercial applications. Trane® Connect™ is our secure, cloud-based customer portal to access your building systems to remotely monitor and manage building systems, and conduct routine maintenance.
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
ARRIS-Hero.png

Customer Story

ARRIS Group, Inc.

ARRIS Group requires 99% uptime for their global data center. Trane provides a system-integrated service with central monitoring of 69 critical points and custom performance metrics. The HVAC includes 54 rooftop units, a 225-ton chiller, and Trane Tracer™ controls.

Location: Georgia

Industry: Data Centers

Products Used: Chillers

Climate: Humid & Hot

Topic: Efficiency

Project Summary

ARRIS Group requires 99 percent or better uptime for their global data center. Trane provided a total system-integrated service solution that includes central monitoring of sixty-nine alarm and event points that are mission critical to delivering uptime. Trane field service technicians deliver a Performance Based Service Agreement with custom defined performance metrics tailored to meet the specific needs of ARRIS. The HVAC system equipment includes fifty-four rooftop units, one air-cooled 225-ton chiller and Trane Tracer™ controls.

Challenge

Uptime is crucial to the operation of a data center and the HVAC system is mission critical to maintain the necessary environment. ARRIS Group, Inc. demands 99 percent or better uptime in order to deliver unmatched reliability for their customers. To achieve and maintain such a high level of uptime, they require:

  • Continuous monitoring of critical alarms and events
  • Immediate response to HVAC system faults
  • Prompt, accurate diagnosis
  • Remote alarm and event remediation
  • Well prepared on-site service

Solution

The Trane Performance Based Agreement, coupled with Trane Central Monitoring, provides 24/7/365 monitoring and alarm routing managed with an automated, state-of-the-art system to alert the Trane remote services center staff of a critical event. Trane technical specialists respond immediately to remotely interrogate the system and perform system fault diagnostics. Trane technical specialists can remotely resolve up to 40 percent of alarms and events without rolling a service truck. If on-site service is needed, Trane field service technicians are well-equipped with the system knowledge needed to expedite repairs. Custom defined performance metrics are tailored to meet customer-specific needs.

Results

The ARRIS Group global data center consistently achieves 99 percent uptime due in large part to their partnership with Trane and the exceptional service provided by Trane remote services.

  • Ninety-nine percent uptime delivers customer satisfaction
  • Sixty percent reduction in operational downtime contributes to the bottom line
  • 50 percent reduction in service truck rolls reduces operating cost
  • Seven minute average response time speeds remediation activities
  • Thirty-nine minute average time to resolution minimizes downtime 

Mark Manning, Facilities/Security Manager, said, “The Trane Performance Based Agreement, coupled with Trane Central Monitoring, has significantly reduced our downtime by more than 60 percent and cut our truck rolls in half, which has improved response time and turnaround time on system repairs. With Trane Central Monitoring we’ve been able to maintain a 99 percent uptime commitment to our customers. Trane Central Monitoring is a critical tool in our business process to insure we meet our business demands. With my local Trane account manager I always know I am in good hands and that tasks will be done 100 percent of the time.”

No matter how mission critical your operation may be, Trane can provide innovative, total system-integrated service solutions to meet your needs.

About ARRIS Group, Inc.

ARRIS Group, Inc. is a global communications technology company specializing in the design and engineering of broadband networks. The 143,000 square-foot facility is home to their corporate headquarters with 3,500 square feet dedicated to their global data center. ARRIS customers demand instantaneous, consistent and reliable access to their data warehouse. The HVAC system is mission critical in maintaining the proper environment necessary to sustain data center operations. ARRIS requires 99 percent or better uptime of their data center operations in order to deliver on this commitment to their customers. HVAC system faults require immediate service response and turnaround time to meet the high standards of customer satisfaction set by ARRIS.

  • City Multi High Rise Residential Regency Install
    VRF: Staying Cool through the Refrigerant Change

    As refrigerant regulations evolve, Trane VRF systems lead with efficiency, flexibility, and sustainability. Learn how the VRF industry is adapting to new regulations.

  • Cold Storage Rental
    6 Ways Cold Storage Rentals Improve Efficiency

    Discover how a refrigerated container rental enhances energy efficiency, reduces costs, and ensures reliable storage for your temperature-sensitive goods.

  • Trane Press Release
    Trane Thermal Management System Innovations Set New Cooling Standards for the Data Center Industry

    Enhanced air-cooled chillers bring larger capacity and higher ambient temperature cooling capabilities to mission critical operations, further expanding Trane’s thermal management systems capabilities.